2.113.24 PMECC_CALLBACK Typedef
C
typedef void (* PMECC_CALLBACK)( uintptr_t context, uint32_t interruptStatus )
Summary
Defines the data type and function signature for the PMECC peripheral callback function.
Description
This data type defines the function signature for the PMECC peripheral callback function. The PMECC peripheral will call back the client's function with this signature when the PMECC interrupt has occurred.
Precondition
PMECC_Initialize must have been called for the given PMECC peripheral instance. Callback must have been registered using PMECC_CallbackRegister().
Parameters
| Param | Description |
|---|---|
| context | Allows the caller to provide a context value (usually a pointerto the callers context for multiple clients) |
| interruptStatus | PMECC interrupt status |
Returns
None.
Example
void pmeccCallback( uintptr_t context, uint32_t interruptStatus )
{
}
PMECC_CallbackRegister(pmeccCallback, (uintptr_t)NULL);
Remarks
None.