2.11.24 CCPx_Compare16bitValueSet Function
C
/* x = CCP instance number */
void CCPx_Compare16bitValueSet( uint16_t count )
Summary
Sets new timer counter value.
Description
This function sets new timer counter value.
Precondition
CCPx_CompareInitialize() function must have been called first.
Parameters
| Param | Description |
|---|---|
| count | new counter value to set |
Returns
None.
Example
uint16_t count = 0x100;
CCP1_CompareInitialize();
CCP1_CompareStart();
CCP1_Compare16bitValueSet(count);
Remarks
The caller must know the number of significant bytes of timer. Counter value is right-aligned.