3.1.11 I2C SMBUS
The I2C SMBUS PLIB support I2C Master, I2C Slave, SMBUS Master and SMBUS Slave modes.
Using the Library
I2C Master mode - The below example uses the I2C peripheral library to write an array of
values to the I2C Serial EEPROM and verify the value written by reading the values back and
comparing it to the value
written.
#include <string.h>
#define LED_ON() LED5_Set()
#define LED_OFF() LED5_Clear()
#define APP_AT24MAC_DEVICE_ADDR 0x0054
#define APP_AT24MAC_MEMORY_ADDR 0x00
#define APP_AT24MAC_MEMORY_ADDR1 0x00
#define APP_TRANSMIT_DATA_LENGTH 6
#define APP_ACK_DATA_LENGTH 1
#define APP_RECEIVE_DUMMY_WRITE_LENGTH 2
#define APP_RECEIVE_DATA_LENGTH 4
static uint8_t testTxData[APP_TRANSMIT_DATA_LENGTH] =
{
APP_AT24MAC_MEMORY_ADDR,APP_AT24MAC_MEMORY_ADDR1,
'M','C','H','P',
};
static uint8_t testRxData[APP_RECEIVE_DATA_LENGTH];
typedef enum
{
APP_STATE_EEPROM_STATUS_VERIFY,
APP_STATE_EEPROM_WRITE,
APP_STATE_EEPROM_WAIT_WRITE_COMPLETE,
APP_STATE_EEPROM_CHECK_INTERNAL_WRITE_STATUS,
APP_STATE_EEPROM_READ,
APP_STATE_EEPROM_WAIT_READ_COMPLETE,
APP_STATE_VERIFY,
APP_STATE_IDLE,
APP_STATE_XFER_SUCCESSFUL,
APP_STATE_XFER_ERROR
} APP_STATES;
typedef enum
{
APP_TRANSFER_STATUS_IN_PROGRESS,
APP_TRANSFER_STATUS_SUCCESS,
APP_TRANSFER_STATUS_ERROR,
APP_TRANSFER_STATUS_IDLE,
} APP_TRANSFER_STATUS;
void APP_I2CCallback(uintptr_t context )
{
APP_TRANSFER_STATUS* transferStatus = (APP_TRANSFER_STATUS*)context;
if(I2C0_ErrorGet() == I2C_ERROR_NONE)
{
if (transferStatus)
{
*transferStatus = APP_TRANSFER_STATUS_SUCCESS;
}
}
else
{
if (transferStatus)
{
*transferStatus = APP_TRANSFER_STATUS_ERROR;
}
}
}
// *****************************************************************************
// *****************************************************************************
// Section: Main Entry Point
// *****************************************************************************
// *****************************************************************************
int main ( void )
{
APP_STATES state = APP_STATE_EEPROM_STATUS_VERIFY;
volatile APP_TRANSFER_STATUS transferStatus = APP_TRANSFER_STATUS_ERROR;
uint8_t ackData = 0;
/* Initialize all modules */
SYS_Initialize ( NULL );
while(1)
{
/* Check the application's current state. */
switch (state)
{
case APP_STATE_EEPROM_STATUS_VERIFY:
/* Register the TWIHS Callback with transfer status as context */
I2C0_CallbackRegister( APP_I2CCallback, (uintptr_t)&transferStatus );
/* Verify if EEPROM is ready to accept new requests */
transferStatus = APP_TRANSFER_STATUS_IN_PROGRESS;
I2C0_Write(APP_AT24MAC_DEVICE_ADDR, &ackData, APP_ACK_DATA_LENGTH);
state = APP_STATE_EEPROM_WRITE;
break;
case APP_STATE_EEPROM_WRITE:
if (transferStatus == APP_TRANSFER_STATUS_SUCCESS)
{
/* Write data to EEPROM */
transferStatus = APP_TRANSFER_STATUS_IN_PROGRESS;
I2C0_Write(APP_AT24MAC_DEVICE_ADDR, &testTxData[0], APP_TRANSMIT_DATA_LENGTH);
state = APP_STATE_EEPROM_WAIT_WRITE_COMPLETE;
}
else if (transferStatus == APP_TRANSFER_STATUS_ERROR)
{
/* EEPROM is not ready to accept new requests.
* Keep checking until the EEPROM becomes ready. */
state = APP_STATE_EEPROM_STATUS_VERIFY;
}
break;
case APP_STATE_EEPROM_WAIT_WRITE_COMPLETE:
if (transferStatus == APP_TRANSFER_STATUS_SUCCESS)
{
/* Read the status of internal write cycle */
transferStatus = APP_TRANSFER_STATUS_IN_PROGRESS;
I2C0_Write(APP_AT24MAC_DEVICE_ADDR, &ackData, APP_ACK_DATA_LENGTH);
state = APP_STATE_EEPROM_CHECK_INTERNAL_WRITE_STATUS;
}
else if (transferStatus == APP_TRANSFER_STATUS_ERROR)
{
state = APP_STATE_XFER_ERROR;
}
break;
case APP_STATE_EEPROM_CHECK_INTERNAL_WRITE_STATUS:
if (transferStatus == APP_TRANSFER_STATUS_SUCCESS)
{
state = APP_STATE_EEPROM_READ;
}
else if (transferStatus == APP_TRANSFER_STATUS_ERROR)
{
/* EEPROM's internal write cycle is not complete. Keep checking. */
transferStatus = APP_TRANSFER_STATUS_IN_PROGRESS;
I2C0_Write(APP_AT24MAC_DEVICE_ADDR, &ackData, APP_ACK_DATA_LENGTH);
}
break;
case APP_STATE_EEPROM_READ:
transferStatus = APP_TRANSFER_STATUS_IN_PROGRESS;
/* Read the data from the page written earlier */
I2C0_WriteRead(APP_AT24MAC_DEVICE_ADDR, &testTxData[0], APP_RECEIVE_DUMMY_WRITE_LENGTH, &testRxData[0], APP_RECEIVE_DATA_LENGTH);
state = APP_STATE_EEPROM_WAIT_READ_COMPLETE;
break;
case APP_STATE_EEPROM_WAIT_READ_COMPLETE:
if (transferStatus == APP_TRANSFER_STATUS_SUCCESS)
{
state = APP_STATE_VERIFY;
}
else if (transferStatus == APP_TRANSFER_STATUS_ERROR)
{
state = APP_STATE_XFER_ERROR;
}
break;
case APP_STATE_VERIFY:
if (memcmp(&testTxData[2], &testRxData[0], APP_RECEIVE_DATA_LENGTH) != 0 )
{
/* It means received data is not same as transmitted data */
state = APP_STATE_XFER_ERROR;
}
else
{
/* It means received data is same as transmitted data */
state = APP_STATE_XFER_SUCCESSFUL;
}
break;
case APP_STATE_XFER_SUCCESSFUL:
{
LED_ON();
break;
}
case APP_STATE_XFER_ERROR:
{
LED_OFF();
break;
}
default:
break;
}
}
}I2C slave mode - The below example uses the I2C peripheral library in slave mode and
emulates an EEPROM of 512
bytes.
#define EEPROM_PAGE_SIZE_BYTES 256
#define EEPROM_PAGE_SIZE_MASK 0xFF
#define EEPROM_SIZE_BYTES 512
typedef enum
{
EEPROM_CMD_WRITE,
EEPROM_CMD_IDLE,
}EEPROM_CMD;
typedef struct
{
/* currentAddrPtr - to allow for sequential read (from the current address) */
uint16_t currentAddrPtr;
/* addrIndex - used to copy 2 bytes of EEPROM memory address */
uint8_t addrIndex;
/* wrBuffer - holds the incoming data from the I2C master */
uint8_t wrBuffer[EEPROM_PAGE_SIZE_BYTES];
/* wrBufferIndex - Index into the wrBuffer[] */
uint16_t wrBufferIndex;
/* wrAddr - indicates the starting address of the EEPROM emulation memory to write to */
volatile uint16_t wrAddr;
/* nWrBytes - indicates the number of bytes to write to EEPROM emulation buffer */
volatile uint8_t nWrBytes;
/* internalWriteInProgress - indicates that EEPROM is busy with internal writes */
bool internalWriteInProgress;
/* eepromCommand - used to trigger write to the EEPROM emulation buffer */
EEPROM_CMD eepromCommand;
}EEPROM_DATA;
EEPROM_DATA eepromData;
uint8_t EEPROM_EmulationBuffer[EEPROM_SIZE_BYTES] =
{
0x00,0x01,0x02,0x03,0x04,0x05,0x06,0x07,0x08,0x09,0x0a,0x0b,0x0c,0x0d,0x0e,0x0f,
0x10,0x11,0x12,0x13,0x14,0x15,0x16,0x17,0x18,0x19,0x1a,0x1b,0x1c,0x1d,0x1e,0x1f,
0x20,0x21,0x22,0x23,0x24,0x25,0x26,0x27,0x28,0x29,0x2a,0x2b,0x2c,0x2d,0x2e,0x2f,
0x30,0x31,0x32,0x33,0x34,0x35,0x36,0x37,0x38,0x39,0x3a,0x3b,0x3c,0x3d,0x3e,0x3f,
0x40,0x41,0x42,0x43,0x44,0x45,0x46,0x47,0x48,0x49,0x4a,0x4b,0x4c,0x4d,0x4e,0x4f,
0x50,0x51,0x52,0x53,0x54,0x55,0x56,0x57,0x58,0x59,0x5a,0x5b,0x5c,0x5d,0x5e,0x5f,
0x60,0x61,0x62,0x63,0x64,0x65,0x66,0x67,0x68,0x69,0x6a,0x6b,0x6c,0x6d,0x6e,0x6f,
0x70,0x71,0x72,0x73,0x74,0x75,0x76,0x77,0x78,0x79,0x7a,0x7b,0x7c,0x7d,0x7e,0x7f,
0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8a,0x8b,0x8c,0x8d,0x8e,0x8f,
0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x9a,0x9b,0x9c,0x9d,0x9e,0x9f,
0xa0,0xa1,0xa2,0xa3,0xa4,0xa5,0xa6,0xa7,0xa8,0xa9,0xaa,0xab,0xac,0xad,0xae,0xaf,
0xb0,0xb1,0xb2,0xb3,0xb4,0xb5,0xb6,0xb7,0xb8,0xb9,0xba,0xbb,0xbc,0xbd,0xbe,0xbf,
0xc0,0xc1,0xc2,0xc3,0xc4,0xc5,0xc6,0xc7,0xc8,0xc9,0xca,0xcb,0xcc,0xcd,0xce,0xcf,
0xd0,0xd1,0xd2,0xd3,0xd4,0xd5,0xd6,0xd7,0xd8,0xd9,0xda,0xdb,0xdc,0xdd,0xde,0xdf,
0xe0,0xe1,0xe2,0xe3,0xe4,0xe5,0xe6,0xe7,0xe8,0xe9,0xea,0xeb,0xec,0xed,0xee,0xef,
0xf0,0xf1,0xf2,0xf3,0xf4,0xf5,0xf6,0xf7,0xf8,0xf9,0xfa,0xfb,0xfc,0xfd,0xfe,0xff,
0x00,0x01,0x02,0x03,0x04,0x05,0x06,0x07,0x08,0x09,0x0a,0x0b,0x0c,0x0d,0x0e,0x0f,
0x10,0x11,0x12,0x13,0x14,0x15,0x16,0x17,0x18,0x19,0x1a,0x1b,0x1c,0x1d,0x1e,0x1f,
0x20,0x21,0x22,0x23,0x24,0x25,0x26,0x27,0x28,0x29,0x2a,0x2b,0x2c,0x2d,0x2e,0x2f,
0x30,0x31,0x32,0x33,0x34,0x35,0x36,0x37,0x38,0x39,0x3a,0x3b,0x3c,0x3d,0x3e,0x3f,
0x40,0x41,0x42,0x43,0x44,0x45,0x46,0x47,0x48,0x49,0x4a,0x4b,0x4c,0x4d,0x4e,0x4f,
0x50,0x51,0x52,0x53,0x54,0x55,0x56,0x57,0x58,0x59,0x5a,0x5b,0x5c,0x5d,0x5e,0x5f,
0x60,0x61,0x62,0x63,0x64,0x65,0x66,0x67,0x68,0x69,0x6a,0x6b,0x6c,0x6d,0x6e,0x6f,
0x70,0x71,0x72,0x73,0x74,0x75,0x76,0x77,0x78,0x79,0x7a,0x7b,0x7c,0x7d,0x7e,0x7f,
0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8a,0x8b,0x8c,0x8d,0x8e,0x8f,
0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x9a,0x9b,0x9c,0x9d,0x9e,0x9f,
0xa0,0xa1,0xa2,0xa3,0xa4,0xa5,0xa6,0xa7,0xa8,0xa9,0xaa,0xab,0xac,0xad,0xae,0xaf,
0xb0,0xb1,0xb2,0xb3,0xb4,0xb5,0xb6,0xb7,0xb8,0xb9,0xba,0xbb,0xbc,0xbd,0xbe,0xbf,
0xc0,0xc1,0xc2,0xc3,0xc4,0xc5,0xc6,0xc7,0xc8,0xc9,0xca,0xcb,0xcc,0xcd,0xce,0xcf,
0xd0,0xd1,0xd2,0xd3,0xd4,0xd5,0xd6,0xd7,0xd8,0xd9,0xda,0xdb,0xdc,0xdd,0xde,0xdf,
0xe0,0xe1,0xe2,0xe3,0xe4,0xe5,0xe6,0xe7,0xe8,0xe9,0xea,0xeb,0xec,0xed,0xee,0xef,
0xf0,0xf1,0xf2,0xf3,0xf4,0xf5,0xf6,0xf7,0xf8,0xf9,0xfa,0xfb,0xfc,0xfd,0xfe,0xff
};
bool APP_SERCOM_I2C_Callback ( I2C_SLAVE_TRANSFER_EVENT event, uintptr_t contextHandle )
{
bool isSuccess = true;
switch(event)
{
case I2C_SLAVE_TRANSFER_EVENT_ADDR_MATCH:
if ((I2C0_TransferDirGet() == I2C_SLAVE_TRANSFER_DIR_WRITE) && (eepromData.internalWriteInProgress == true))
{
/* EEPROM is busy. Send NAK */
isSuccess = false;
}
else
{
/* Reset the indexes */
eepromData.addrIndex = 0;
eepromData.wrBufferIndex = 0;
}
break;
case I2C_SLAVE_TRANSFER_EVENT_RX_READY:
/* Read the data sent by I2C Master */
if (eepromData.addrIndex < 2)
{
((uint8_t*)&eepromData.currentAddrPtr)[eepromData.addrIndex++] = I2C0_ReadByte();
}
else
{
eepromData.wrBuffer[(eepromData.wrBufferIndex & EEPROM_PAGE_SIZE_MASK)] = I2C0_ReadByte();
eepromData.wrBufferIndex++;
}
break;
case I2C_SLAVE_TRANSFER_EVENT_TX_READY:
/* Provide the EEPROM data requested by the I2C Master */
I2C0_WriteByte(EEPROM_EmulationBuffer[eepromData.currentAddrPtr++]);
if (eepromData.currentAddrPtr >= EEPROM_SIZE_BYTES)
{
eepromData.currentAddrPtr = 0;
}
break;
case I2C_SLAVE_TRANSFER_EVENT_STOP_BIT_RECEIVED:
if (eepromData.wrBufferIndex > 0)
{
if (eepromData.wrBufferIndex > EEPROM_PAGE_SIZE_BYTES)
{
eepromData.wrBufferIndex = EEPROM_PAGE_SIZE_BYTES;
}
eepromData.wrAddr = eepromData.currentAddrPtr;
eepromData.nWrBytes = eepromData.wrBufferIndex;
/* Update the current address pointer to allow for sequential read */
eepromData.currentAddrPtr += eepromData.wrBufferIndex;
/* Reset the indexes */
eepromData.addrIndex = 0;
eepromData.wrBufferIndex = 0;
/* Set busy flag to send NAK for any write requests */
eepromData.internalWriteInProgress = true;
eepromData.eepromCommand = EEPROM_CMD_WRITE;
}
break;
default:
break;
}
return isSuccess;
}
void EEPROM_StateMachine(void)
{
switch(eepromData.eepromCommand)
{
case EEPROM_CMD_WRITE:
memcpy(&EEPROM_EmulationBuffer[eepromData.wrAddr], &eepromData.wrBuffer[0], eepromData.nWrBytes);
eepromData.internalWriteInProgress = false;
eepromData.eepromCommand = EEPROM_CMD_IDLE;
break;
case EEPROM_CMD_IDLE:
/* Do Nothing */
break;
}
}
int main ( void )
{
/* Initialize all modules */
SYS_Initialize ( NULL );
eepromData.eepromCommand = EEPROM_CMD_IDLE;
I2C0_CallbackRegister(APP_SERCOM_I2C_Callback, 0);
while ( true )
{
EEPROM_StateMachine();
}
/* Execution should not come here during normal operation */
return ( EXIT_FAILURE );
}SMBUS Host mode - The below example uses the SMBUS peripheral library and demonstrates how
application can use the various APIs available to read and write data when the peripheral is
configured in master
mode.
#define I2C_SLAVE_ADDR 0x54
typedef enum
{
HOST_STATE_WRITE_BYTE = 0,
HOST_STATE_WRITE_WORD,
HOST_STATE_WRITE_BLOCK,
HOST_STATE_READ_BYTE,
HOST_STATE_READ_WORD,
HOST_STATE_READ_BLOCK,
HOST_STATE_WRITE_READ_BLOCK,
HOST_STATE_WAIT_FOR_TRANSFER_DONE,
HOST_STATE_ERROR,
HOST_STATE_SUCCESS,
}HOST_STATE;
typedef enum
{
HOST_CMD_WRITE_BYTE,
HOST_CMD_WRITE_WORD,
HOST_CMD_WRITE_BLOCK,
HOST_CMD_READ_BYTE,
HOST_CMD_READ_WORD,
HOST_CMD_READ_BLOCK,
HOST_CMD_WRITE_READ_BLOCK,
}HOST_CMD;
volatile bool transferDone = false;
volatile uint32_t nBytesRead = 0;
bool blockRead = false;
uint32_t nBytesRequested = 0;
uint8_t wrBuffer[50] = {0};
uint8_t rdBuffer[50] = {0};
volatile HOST_STATE state = HOST_STATE_WRITE_BYTE;
HOST_STATE nextState;
void i2cSMB0HostEventHandler (I2C_SMB_HOST_TRANSFER_EVENT event, uintptr_t contextHandle)
{
switch(event)
{
case I2C_SMB_HOST_TRANSFER_EVENT_RX_READY:
nBytesRead = I2CSMB0_HostBufferRead(rdBuffer);
break;
case I2C_SMB_HOST_TRANSFER_EVENT_DONE:
transferDone = true;
break;
case I2C_SMB_HOST_TRANSFER_EVENT_ERROR:
state = HOST_STATE_ERROR;
break;
default:
break;
}
}
int main ( void )
{
uint32_t i = 0;
uint32_t data = 1;
/* Initialize all modules */
SYS_Initialize ( NULL );
I2CSMB0_HostCallbackRegister(i2cSMB0HostEventHandler, 0);
while (1)
{
switch(state)
{
case HOST_STATE_WAIT_FOR_TRANSFER_DONE:
if (transferDone == true)
{
transferDone = false;
state = nextState;
if (nBytesRequested > 0)
{
i = 0;
data = 1;
if (blockRead == true)
{
// for block reads, the first byte indicates the number of bytes transmitted by the slave
nBytesRead = rdBuffer[i++];
blockRead = false;
}
if (nBytesRead != nBytesRequested)
{
state = HOST_STATE_ERROR;
break;
}
while (nBytesRequested--)
{
if (rdBuffer[i++] != data++)
{
state = HOST_STATE_ERROR;
break;
}
}
nBytesRequested = 0;
}
}
break;
case HOST_STATE_WRITE_BYTE:
wrBuffer[0] = 1;
I2CSMB0_HostWriteByte(I2C_SLAVE_ADDR, HOST_CMD_WRITE_BYTE, wrBuffer);
state = HOST_STATE_WAIT_FOR_TRANSFER_DONE;
nextState = HOST_STATE_READ_BYTE;
break;
case HOST_STATE_READ_BYTE:
nBytesRequested = 1;
I2CSMB0_HostReadByte(I2C_SLAVE_ADDR, HOST_CMD_READ_BYTE);
state = HOST_STATE_WAIT_FOR_TRANSFER_DONE;
nextState = HOST_STATE_WRITE_WORD;
break;
case HOST_STATE_WRITE_WORD:
wrBuffer[0] = 1;
wrBuffer[1] = 2;
I2CSMB0_HostWriteWord(I2C_SLAVE_ADDR, HOST_CMD_WRITE_WORD, wrBuffer);
state = HOST_STATE_WAIT_FOR_TRANSFER_DONE;
nextState = HOST_STATE_READ_WORD;
break;
case HOST_STATE_READ_WORD:
nBytesRequested = 2;
I2CSMB0_HostReadWord(I2C_SLAVE_ADDR, HOST_CMD_READ_WORD);
state = HOST_STATE_WAIT_FOR_TRANSFER_DONE;
nextState = HOST_STATE_WRITE_BLOCK;
break;
case HOST_STATE_WRITE_BLOCK:
for (uint32_t i = 0; i < 32; i++)
{
wrBuffer[i] = i+1;
}
I2CSMB0_HostWriteBlock(I2C_SLAVE_ADDR, HOST_CMD_WRITE_BLOCK, wrBuffer, 32);
state = HOST_STATE_WAIT_FOR_TRANSFER_DONE;
nextState = HOST_STATE_READ_BLOCK;
break;
case HOST_STATE_READ_BLOCK:
nBytesRequested = 32;
blockRead = true;
I2CSMB0_HostReadBlock(I2C_SLAVE_ADDR, HOST_CMD_READ_BLOCK);
state = HOST_STATE_WAIT_FOR_TRANSFER_DONE;
nextState = HOST_STATE_WRITE_READ_BLOCK;
break;
case HOST_STATE_WRITE_READ_BLOCK:
nBytesRequested = 32;
blockRead = true;
I2CSMB0_HostWriteReadBlock(I2C_SLAVE_ADDR, HOST_CMD_WRITE_READ_BLOCK, wrBuffer, 32);
state = HOST_STATE_WAIT_FOR_TRANSFER_DONE;
nextState = HOST_STATE_SUCCESS;
break;
case HOST_STATE_SUCCESS:
break;
case HOST_STATE_ERROR:
break;
}
}
/* Execution should not come here during normal operation */
return ( EXIT_FAILURE );
}SMBUS Target mode - The below example uses the SMBUS peripheral library and demonstrates
how application can use the various APIs available to read and write data when the
peripheral is configured in slave
mode.
typedef enum
{
HOST_CMD_WRITE_BYTE,
HOST_CMD_WRITE_WORD,
HOST_CMD_WRITE_BLOCK,
HOST_CMD_READ_BYTE,
HOST_CMD_READ_WORD,
HOST_CMD_READ_BLOCK,
HOST_CMD_WRITE_READ_BLOCK,
}HOST_CMD;
volatile uint8_t targetRxBuffer[100];
volatile uint8_t targetTxBuffer[100];
volatile uint32_t nBytesRead = 0;
volatile uint32_t nDataBytes = 0;
volatile HOST_CMD command;
bool i2cSMB0TargetEventHandler (I2C_SMB_TARGET_TRANSFER_EVENT event, uintptr_t contextHandle)
{
switch (event)
{
case I2C_SMB_TARGET_TRANSFER_EVENT_RX_READY:
nBytesRead = I2CSMB0_TargetBufferRead((void*)targetRxBuffer);
command = targetRxBuffer[1];
if (command == HOST_CMD_WRITE_BYTE)
{
nDataBytes = 1;
targetTxBuffer[0] = targetRxBuffer[2];
}
else if (command == HOST_CMD_WRITE_WORD)
{
nDataBytes = 2;
targetTxBuffer[0] = targetRxBuffer[2];
targetTxBuffer[1] = targetRxBuffer[3];
}
else if ((command == HOST_CMD_WRITE_BLOCK) || (command == HOST_CMD_WRITE_READ_BLOCK))
{
nDataBytes = targetRxBuffer[2];
targetTxBuffer[0] = nDataBytes;
memcpy((void*)&targetTxBuffer[1], (void*)&targetRxBuffer[3], nDataBytes);
nDataBytes = nDataBytes + 1;
}
break;
case I2C_SMB_TARGET_TRANSFER_EVENT_TX_READY:
I2CSMB0_TargetBufferWrite((void*)targetTxBuffer, nDataBytes);
break;
case I2C_SMB_TARGET_TRANSFER_EVENT_ERROR:
break;
case I2C_SMB_TARGET_TRANSFER_EVENT_DONE:
break;
default:
break;
}
return true;
}
int main ( void )
{
/* Initialize all modules */
SYS_Initialize ( NULL );
I2CSMB0_TargetCallbackRegister(i2cSMB0TargetEventHandler, 0);
I2CSMB0_TargetStart();
while (1)
{
/* Do nothing */
}
/* Execution should not come here during normal operation */
return ( EXIT_FAILURE );
}Library Interface
I2C Mode
| Name | Description | Master mode | Slave mode |
|---|---|---|---|
| I2CSMBx_Initialize | Initializes given instance of I2C SMBUS peripheral. | Yes | Yes |
| I2CSMBx_Read | Reads data from the slave. | Yes | No |
| I2CSMBx_Write | Writes data to the slave. | Yes | No |
| I2CSMBx_WriteRead | Write and Read data from I2C Slave. | Yes | No |
| I2CSMBx_IsBusy | Returns the Peripheral busy status. | Yes | Yes |
| I2CSMBx_ErrorGet | Returns the I2C error that occurred on the bus. | Yes | Yes |
| I2CSMBx_TransferSetup | Dynamic setup of I2C Peripheral. | Yes | No |
| I2CSMBx_CallbackRegister | Sets the pointer to the function (and it's context) to be called when the given I2C's transfer events occur. | Yes | Yes |
| I2CSMBx_ReadByte | Read the received I2C byte | No | Yes |
| I2CSMBx_WriteByte | Write a data byte to I2C master | No | Yes |
| I2CSMBx_TransferDirGet | Returns the I2C transfer direction. | No | Yes |
| I2CSMBx_LastByteAckStatusGet | Returns the ACK status of the last byte written to the I2C master. | No | Yes |
| I2CSMBx_StatusFlagsGet | Returns the status register | No | Yes |
| I2CSMBx_StatusFlagsReset | Resets the status register bits | No | Yes |
| I2CSMBx_TransferAbort | Aborts an ongoing transfer | Yes | No |
| Name | Type | Description | Master mode | Slave mode |
|---|---|---|---|---|
| I2C_ERROR | Enum | Defines the possible errors that the I2C peripheral can generate in I2C master mode. | Yes | No |
| I2C_CALLBACK | Typedef | Defines the data type and function signature for the I2C peripheral callback function in I2C master mode. | Yes | No |
| I2C_SLAVE_TRANSFER_EVENT | Enum | Defines the enum for the I2C slave transfer event | No | Yes |
| I2C_SLAVE_TRANSFER_DIR | Enum | Defines the enum for I2C data transfer direction | No | Yes |
| I2C_SLAVE_ERROR | Enum | Defines errors associated with I2C in slave mode | No | Yes |
| I2C_SLAVE_CALLBACK | Typedef | Defines the data type and function signature for the I2C Slave callback function. | No | Yes |
| I2C_SLAVE_ACK_STATUS | Enum | Defines the enum for the I2C slave acknowledgment. | No | Yes |
| I2C_TRANSFER_SETUP | Struct | I2C transfer setup data structure | Yes | No |
SMBUS Mode
| Name | Description | Host Mode | Target Mode |
|---|---|---|---|
| I2CSMBx_Initialize | Initializes given instance of I2C SMBUS peripheral. | Yes | Yes |
| I2CSMBx_HostReadByte | Reads a data byte from slave | Yes | No |
| I2CSMBx_HostReadWord | Reads a data word from slave | Yes | No |
| I2CSMBx_HostWriteByte | Writes data to the slave. | Yes | No |
| I2CSMBx_HostWriteBlock | Writes a block of data to the slave. | Yes | No |
| I2CSMBx_HostReadBlock | Reads a block of data from the slave | Yes | No |
| I2CSMBx_HostWriteWord | Writes word data to the slave. | Yes | No |
| I2CSMBx_HostWriteReadBlock | Writes block followed by a read block from the slave | Yes | No |
| I2CSMBx_HostWriteBlock | Writes a block of data to the slave. | Yes | No |
| I2CSMBx_HostTransferSetup | Dynamic setup of I2C Peripheral in SMBUS host mode | Yes | No |
| I2CSMBx_HostTransferCountGet | Returns the transfer count for the last transfer | Yes | No |
| I2CSMBx_HostIsBusy | Returns the Peripheral busy status. | Yes | No |
| I2CSMBx_HostErrorGet | Returns the I2C error that occurred on the bus. | Yes | No |
| I2CSMBx_HostCallbackRegister | Sets the pointer to the function (and it's context) to be called when the given I2C's transfer events occur. | Yes | No |
| I2CSMBx_HostBufferRead | Reads data from the internal buffer and into the application buffer | Yes | No |
| I2CSMBx_TargetTransferDirGet | Returns the I2C transfer direction. | No | Yes |
| I2CSMBx_TargetStart | Configures the DMA and starts the target in receive mode | No | Yes |
| I2CSMBx_TargetIsBusy | Returns the Peripheral busy status. | No | Yes |
| I2CSMBx_TargetErrorGet | Returns the I2C error that occurred on the bus. | No | Yes |
| I2CSMBx_TargetCallbackRegister | Sets the pointer to the function (and it's context) to be called when the given I2C's transfer events occur. | No | Yes |
| I2CSMBx_TargetBufferWrite | Copies the data to be transmitted into the PLIBs internal buffer | No | Yes |
| I2CSMBx_TargetBufferRead | Reads the received data from internal buffer into the application buffer | No | Yes |
| Name | Type | Description | Host mode | Target mode |
|---|---|---|---|---|
| I2C_SMB_HOST_TRANSFER_SETUP | Struct | I2C Transfer Setup Data Structure | Yes | No |
| I2C_SMB_HOST_TRANSFER_EVENT | Enum | Defines the enum for the I2C SMBUS host transfer events. | Yes | No |
| I2C_SMB_HOST_ERROR | Macro |
Defines macros associated with I2C error in SMBUS Host mode | Yes | No |
| I2C_SMB_HOST_CALLBACK | Typedef | Defines the data type and function signature for the I2C SMBUS host mode callback function. | Yes | No |
| I2C_SMB_TARGET_TRANSFER_EVENT | Enum | Defines the enum for the I2C SMBUS target transfer events | No | Yes |
| I2C_SMB_TARGET_TRANSFER_DIR | Enum | Defines the enum for the I2C SMBUS Target mode transfer direction | No | Yes |
| I2C_SMB_TARGET_ERROR | Macro | Defines macros associated with I2C error in SMBUS Target mode | No | Yes |
| I2C_SMB_TARGET_CALLBACK | Typedef | Defines the data type and function signature for the I2C SMBUS Target mode callback function. | No | Yes |