2.112.7 I2CSMBx_TransferSetup Function
C
/* x = I2C SMBUS peripheral instance number */
/* I2C master mode */
bool I2CSMBx_TransferSetup(I2C_TRANSFER_SETUP* setup, uint32_t srcClkFreq )
Summary
Dynamic setup of I2C Peripheral.
Description
This API is generally used when there are multiple clients on the same I2C bus having different I2C clock speed. In such a case, the I2CSMBx_TransferSetup API must be called to set the appropriate I2C bus speed before starting the I2C transfer for the I2C slave.
Precondition
I2CSMBx_Initialize must have been called for the associated I2C instance. The transfer status should not be busy.
Parameters
| Param | Description |
|---|---|
| setup | Pointer to the structure containing the transfer setup. |
| srcClkFreq | I2C Peripheral Clock Source Frequency. |
Returns
true - Transfer setup was updated Successfully.
false - Failure while updating transfer setup.
Example
I2C_TRANSFER_SETUP setup; setup.clkSpeed = 400000; // Make sure that the I2C is not busy before changing the I2C clock frequency if (I2CSMB0_IsBusy() == false) { if (I2CSMB0_TransferSetup( &setup, 0 ) == true) { // Transfer Setup updated successfully } }
Remarks
srcClkFreq overrides any change in the peripheral clock frequency. If configured to zero PLIB takes the peripheral clock frequency from MCC.