2.112.31 I2CSMBx_TargetIsBusy Function
C
/* x = I2C SMBUS peripheral instance number */
/* I2C SMBUS Target mode */
bool I2CSMBx_TargetIsBusy(void)
Summary
Returns the Peripheral busy status.
Description
This function returns true if the I2CSMBx module is not in idle mode.
Precondition
I2CSMBx_Initialize must have been called for the associated I2C instance.
Parameters
None.
Returns
true - Busy
false - Not busy
Example
// wait for the current transfer to complete while(I2CSMB0_TargetIsBusy());
Remarks
None.