5.7.5 Options for Controlling Warning and Errors
Warnings are diagnostic messages that report constructions that are not inherently erroneous, but that are risky or suggest there may have been an error.
You can request many specific warnings with options beginning -W; for
example, -Wimplicit, to request warnings on implicit declarations. Each
of these specific warning options also has a negative form beginning
-Wno- to turn off warnings; for example,
-Wno-implicit. This manual lists only one of the two forms,
whichever is not the default.
The options shown in the tables below are the more commonly used warning options that control messages issued by the compile. In the (linked) sections that follow, the options that affect warnings generally are discussed.
| Option | Definition |
|---|---|
-fsyntax-only |
Check the code for syntax, but don’t do anything beyond that. |
-pedantic |
Issue all the warnings demanded by strict ANSI C. Reject all programs that use forbidden extensions. |
-pedantic-errors |
Like -pedantic, except that errors are produced
rather than warnings. |
-w |
Inhibit all warning messages. |
-Wall |
Enable all warnings about constructions that some users consider questionable, and that are easy to avoid, even in conjunction with macros. |
-Waddress |
Warn about suspicious uses of memory addresses. These include using
the address of a function in a conditional expression, such as
void func(void); if (func), and
comparisons against the memory address of a string literal, such as if
(x == "abc"). Such uses typically indicate a
programmer error: the address of a function always evaluates to true, so
their use in a conditional usually indicates that the programmer forgot
the parentheses in a function call; and comparisons against string
literals result in unspecified behavior and are not portable in C, so
they usually indicate that the programmer intended to use
strcmp. |
-Warray-bounds |
When combined with -02 or greater, warns for many instances
out-of-bounds array indices and pointer offsets. This feature cannot
detect all cases. Enabled with -Wall command. |
-Wchar-subscripts |
Warn if an array subscript has type char. |
|
|
Warn whenever a comment-start sequence /* appears in
a /*comment, or whenever a Backslash-Newline appears in
a // comment. |
-Wdiv-by-zero |
Warn about compile-time integer division by zero. To
inhibit the warning messages, use -Wno-div-by-zero.
Floating-point division by zero is not warned about, as it can be a
-legitimate way of obtaining infinities and NaNs.This is the default. |
-Wformat |
Check calls to printf and scanf,
etc., to make sure that the arguments supplied have types appropriate to
the format string specified. |
-Wimplicit |
Equivalent to specifying both
-Wimplicit-int and
-Wimplicit-function-declaration. |
-Wimplicit-function-
declaration |
Give a warning whenever a function is used before being declared. |
-Wimplicit-int |
Warn when a declaration does not specify a type. |
-Wmain |
Warn if the type of main is suspicious.
main should be a function with external linkage,
returning int, taking either zero, two, or three
arguments of appropriate types. |
-Wmissing-braces |
Warn if an aggregate or union initializer is not fully
bracketed. In the following example, the initializer for
a is not fully bracketed, but that for
b is fully bracketed.
|
-Wmultistatement-macros |
Warns for unsafe macro expansion as a body of a statement such as if,
else, while, switch, or for. Enabled with -Wall
command. |
-Wno-multichar |
Warn if a multi-character character
constant is used. Usually, such constants are typographical errors.
Since they have implementation-defined values, they should not be used
in portable code. The following example illustrates the use of a
multi-character character constant:
|
-Wparentheses |
Warn if parentheses are omitted in certain contexts, such as when there is an assignment in a context where a truth value is expected, or when operators are nested whose precedence people often find confusing. |
-Wreturn-type |
Warn whenever a function is defined with a return-type that defaults
to int. Also warn about any return
statement with no return-value in a function whose return-type is not
void. |
-Wsequence-point |
Warn about code that may have undefined semantics because
of violations of sequence point rules in the C standard. The C standard defines the order in which expressions in a C
program are evaluated in terms of sequence points, which represent a
partial ordering between the execution of parts of the program:
those executed before the sequence point and those executed after
it. These occur after the evaluation of a full expression (one which
is not part of a larger expression), after the evaluation of the
first operand of a It is not specified when between sequence points modifications to the values of objects take effect. Programs whose behavior depends on this have undefined behavior. The C standard specifies that “Between the previous and next sequence point, an object shall have its stored value modified, at most once, by the evaluation of an expression. Furthermore, the prior value shall be read only to determine the value to be stored.” If a program breaks these rules, the results on any particular implementation are entirely unpredictable. Examples of code with undefined behavior are
|
-Wsizeof-pointer-div |
Warns for suspicious divisions of the size of a pointer by the size of the elements it points to, which looks like the usual way to compute the array size but won't work out correctly with pointers. |
-Wswitch |
Warn whenever a switch statement has an index of
enumeral type and lacks a case for one or more of the named codes of
that enumeration. The presence of a default label prevents this warning.
case labels outside the enumeration range also
provoke warnings when this option is used. |
-Wsystem-headers |
Print warning messages for constructs found in system header files.
Warnings from system headers are normally suppressed on the assumption
that they usually do not indicate real problems and would only make the
compiler output harder to read. Using this command line option tells the
compiler to emit warnings from system headers as if they occurred in
user code. However, note that using -Wall in
conjunction with this option does not warn about unknown pragmas in
system headers. For that, -Wunknown-pragmas must also
be used. |
-Wtrigraphs |
Warn if any trigraphs are encountered (assuming they are enabled). |
-Wuninitialized |
Warn if an automatic variable is used without first being
initialized. These warnings are possible only when optimization is enabled, because they require data flow information that is computed only when optimizing. These
warnings occur only for variables that are candidates for register
allocation. Therefore, they do not occur for a variable that is
declared Note that there may be no warning about a variable that is used only to compute a value that itself is never used, because such computations may be deleted by data flow analysis before the warnings are printed. |
-Wunknown-pragmas |
Warn when a #pragma directive is encountered which
is not understood by the compiler. If this command line option is used,
warnings will even be issued for unknown pragmas in system header files.
This is not the case if the warnings were only enabled by the
-Wall command line option. |
-Wunused |
Warn whenever a variable is unused aside from its declaration,
whenever a function is declared static but never defined, whenever a
label is declared but not used, and whenever a statement computes a
result that is explicitly not used. In order to get a warning about an
unused function parameter, both Casting an
expression to void suppresses this warning for an expression.
Similarly, the |
-Wunused-function |
Warn whenever a static function is declared but not defined or a non-inline static function is unused. |
-Wunused-label |
Warn whenever a label is declared but not used. To suppress this
warning, use the unused attribute. |
-Wunused-parameter |
Warn whenever a function parameter is unused aside from its
declaration. To suppress this warning, use the unused
attribute. |
-Wunused-variable |
Warn whenever a local variable or non-constant static variable is
unused aside from its declaration. To suppress this warning, use the
unused attribute. |
-Wunused-value |
Warn whenever a statement computes a result that is explicitly not used. To suppress this warning, cast the expression to void. |
The following -W options are not implied by -Wall. Some
of them warn about constructions that users generally do not consider questionable, but
which you might occasionally wish to check for. Others warn about constructions that are
necessary or hard to avoid in some cases, and there is no simple way to modify the code
to suppress the warning.
| Option | Definition |
|---|---|
|
(formerly) |
Enable extra warning flags that are not enabled by
-Wall. |
-Waggregate-return |
Warn if any functions that return structures or unions are defined or called. |
-Wbad-function-cast |
Warn whenever a function call is cast to a non-matching type. For
example, warn if int foof() is cast to anything
*. |
-Wcast-align |
Warn whenever a pointer is cast, such that the required alignment of
the target is increased. For example, warn if a char *
is cast to an int *. |
-Wcast-qual |
Warn whenever a pointer is cast, so as to remove a type qualifier
from the target type. For example, warn if a const char
* is cast to an ordinary char *. |
-Wconversion |
Warn if a prototype causes a type conversion that is
different from what would happen to the same argument in the absence of
a prototype. This includes conversions of fixed point to floating and
vice versa, and conversions changing the width or signedness of a fixed
point argument, except when the same as the default promotion. Also, warn if a negative integer constant expression is
implicitly converted to an unsigned type. For example, warn about
the assignment |
-Werror |
Make all warnings into errors. |
-Winline |
Warn if a function can not be inlined, and either it was declared as
inline, or else the -finline-functions option was
given. |
-Wlarger-than-len |
Warn whenever an object of larger than len bytes is
defined. |
|
|
Warn if long long type is used. This is default. To
inhibit the warning messages, use -Wno-long-long. Flags
-Wlong-long and -Wno-long-long are
taken into account only when -pedantic flag is
used. |
-Wmissing-declarations |
Warn if a global function is defined without a previous declaration. Do so even if the definition itself provides a -prototype. |
-Wmissing- format-attribute |
If -Wformat is enabled, also warn about functions
that might be candidates for format attributes. Note these are only
possible candidates, not absolute ones. This option has no effect unless
-Wformat is enabled. |
-Wmissing-noreturn |
Warn about functions that might be candidates for attribute
noreturn. These are only possible candidates, not
absolute ones. Care should be taken to manually verify functions. In
fact, do not ever return before adding the noreturn
attribute, otherwise subtle code generation bugs could be
introduced. |
-Wmissing-prototypes |
Warn if a global function is defined without a previous prototype declaration. This warning is issued even if the definition itself provides a prototype (this option can be used to detect global functions that are not declared in header files). |
-Wnested-externs |
Warn if an extern declaration is encountered within
a function. |
-Wno-deprecated- declarations |
Do not warn about uses of functions, variables and types marked as
deprecated by using the deprecated attribute. |
-Wpadded |
Warn if padding is included in a structure, either to align an element of the structure or to align the whole structure. |
-Wpointer-arith |
Warn about anything that depends on the size of a function type or of
void. The compiler assigns these types a size of 1,
for convenience in calculations with void *pointers and
pointers to functions. |
-Wredundant-decls |
Warn if anything is declared more than once in the same scope, even in cases where multiple declaration is valid and changes nothing. |
-Wshadow |
Warn whenever a local variable shadows another local variable. |
|
|
Warn when a comparison between signed and unsigned values could
produce an incorrect result when the signed value is converted to
unsigned. This warning is also enabled by -W. To get
the other warnings of -W without this warning, use
-W -Wno-sign-compare. |
-Wstrict-prototypes |
Warn if a function is declared or defined without specifying the argument types (an old-style function definition is permitted without a warning if preceded by a declaration which specifies the argument types). |
-Wtraditional |
Warn about certain constructs that behave differently in traditional
and ANSI C.
|
-Wundef |
Warn if an undefined identifier is evaluated in an
#if -directive. |
-Wwrite-strings |
Give string constants the type const char[length] so
that copying the address of one into a non-const char *
pointer gets a warning. At compile time, these warnings help you find
code that you can try to write into a string constant, but only if you
have been very careful about using const in
declarations and prototypes. Otherwise, it’s just a nuisance, which is
why -Wall does not request these warnings. |