11.1.8.9 12-bit ADC Characteristics

Table 11-54. ADC Power Supply and Voltage Reference Input Characteristics
SymbolParameterConditionsMinMaxUnit
VDDANASupply voltage range (VDDANA)–3.03.60V
IDDANACurrent consumption (VDDANA)(1)Low speed – fS ≤ 500 kS/s ADC_ACR.IBCTL = (00)2–1.0mA
Full speed – fS ≤ 1 MS/s ADC_ACR.IBCTL = (01)2–1.8mA
VADVREFPADVREFP input voltage range(2)–2.4VDDANAV
RADVREFPADVREFP input resistance to ground(1)ADC on7.212kΩ
ADC off1–MΩ
CADVREFPRequired bypass capacitor on ADVREFP–1–μF
  1. Simulation data
  2. The ADVREFN pin must be connected to the PCB ground plane.
Table 11-55. ADC Timing Characteristics
SymbolParameterConditionsMinMaxUnit
fCKADCADC clock frequency(1)Low speed – fS ≤ 500 kS/s ADC_ACR.IBCTL = (00)20.110MHz
Full speed – fS ≤ 1 MS/s ADC_ACR.IBCTL = (01)20.220MHz
tCONVADC conversion time(2)–20–tCKADC
fSSampling rate(1)(3)Low speed – fS ≤ 500 kS/s ADC_ACR.IBCTL = (00)2–0.5MS/s
Full speed – fS ≤ 1 MS/s ADC_ACR.IBCTL = (01)2–

1

MS/s
tSTARTStart-up time(4)––5μs
tTRACKTrack and hold time(4)(5)–300–ns
Note:
  1. ADC_ACR.IBCTL defaults to (00)2 at reset, therefore fCKADC and fS are limited to 10 MHz and 500 kS/s, respectively, at reset. Program ADC_ACR.IBCTL to (01)2 to use the ADC at up to 20 MHz and 1 MS/s.
  2. tCONV = tCH + tTRACK + 14 x tCKADC with tCKADC = 1 / fCKADC.

    tCH = 0 when the ADC operates in the same input mode (Single-ended, Pseudo-differential or Differential) for the current conversion than for the previous one.

    tCH = 2 when the ADC input mode is changed to perform the current conversion.

  3. fS = 1 / tCONV
  4. Simulation data
  5. See Track and Hold Time versus Source Impedance – Sampling Rate.
Table 11-56. ADC Analog Input Characteristics
SymbolParameterConditionsMinMaxUnit
VFSAnalog input full scale range (1)ADC_CCR.DIFFx = 00VADVREFPV

ADC_CCR.DIFFx = 1

-VADVREFP

VADVREFP

V
VINCMCommon mode input range in Differential mode(2)ADC_CCR.DIFFx = 10.4 x

VDDANA

0.6 x * VDDANAV

CS

ADC sampling capacitance(3)

––3pF
CP_ADxADx input parasitic capacitance(3)(4)ADx pin configured as analog input–7pF
RON

Internal series resistor(3)(4)

––2kΩ
ZINCommon mode input impedance(3)(5)On ADx pin1 / (fS.CS)–Ω
Note:
  1. VFS = (VADx - VGNDANA) in Single-ended mode, VFS = (VADx - VAD11) in Pseudo-differential mode, and VFS = (VADx - VADx+1) in Differential mode.
  2. VINCM = (VADx + VADx+1) / 2
  3. Simulation data
  4. With respect to the equivalent model of Figure 11-40
  5. Assuming conversion on one single channel
Figure 11-39. Acquisition Path Block Diagram

For tracking time calculation, during the sampling phase of the converter, this acquisition path can be reduced to the equivalent model provided in the following figure, where:

  • RON = RMUX + RS
  • CP_ADX = CPX + CP_MUX
Figure 11-40. Equivalent Model of the Acquisition Path

See Track and Hold Time versus Source Impedance – Sampling Rate for further details on how to use this model.

In the following table, unless otherwise specified, the specifications are provided for two speed operating ranges.

  • Source resistance = 50 Ω
  • ADC_EMR.OSR<2:0> = (000)2
  • Low-speed
    • fCKADC = 10 MHz, fS = 500 kS/s
    • ADC_ACR.IBCTL = (00)2
  • High-speed
    • fCKADC = 20 MHz, fS = 1 MS/s
    • ADC_ACR.IBCTL = (01)2
Table 11-57. Static Performance Characteristics
SymbolParameterConditionsMinMaxUnit
RESADCNative ADC resolution–12Bit
INLIntegral non-linearity–-33LSB
DNLDifferential non-linearity–

-2

2

LSB
OEOffset error–-4

4

LSB
GEGain error–-44LSB
Note:
  1. In this table, errors are expressed in LSB where:
    • LSB = VADVREF / 212 in Single-ended mode (ADC_CCR.DIFFx = 0 and ADC_PDR.PDIFFx = 0)
    • LSB = VADVREF / 211 in Differential or Pseudo-differential mode (ADC_CCR.DIFFx = 1)
  2. Error with respect to the best fit line method