4.4 Running Auto Programming
(Ask a Question)To run Auto programming, perform the following steps:
- Press 3 in PuTTY.
The PuTTY notifies to erase the device using FlashPro and power-cycle the board, see the
following figure.
Figure 4-10. Notifying ERASE Action 
- Using FlashPro, erase the device and
power-cycle the board.
All the LEDs stop glowing for a few seconds, which indicates that the auto programming is in progress. The highest programming image version is selected from the first two available images in external SPI Flash for auto programming. In this case, it is version 2 (
update_image_v2.spi).PuTTY displays the updated design version, see the following figure.Figure 4-11. Successful Auto Programming 
This concludes running the Auto programming feature.