4.5 Running IAP
(Ask a Question)To run IAP, perform the following steps:
- Press 4, IAP program by Index. After around 28 seconds, the IAP with image at index 2 is executed successfully and the design version 05 is displayed, see the following figure.
Figure 4-12. Successful IAP at Index 2 
- Press 5, IAP program by address. After around 28 seconds, the IAP with the image at address 0x1400000 is executed successfully and the design version 05 is displayed, see the following figure.
Figure 4-13. Successful IAP by Address 
This concludes running the IAP feature.
For information about programming the on-board SPI Flash using the fabric logic, see Appendix 1: Programming On-board SPI Flash using the Fabric Logic through the Host Loader.