5.2.2 Get Connection Status (GK)
Format: GK
To obtain the current connection status of the RNBD350 module, use the “Get Connection Status” command, GK.
This command does not require any input parameters. Depending on the module's current connection status, the command provides different outputs:
- If the RNBD350 module is not currently connected to any device and the user uses the command without the optional parameter, the output will be “none”.
- If the RNBD350 module is connected to a device, the
GKcommand returns the following connection information:- <Peer BT Address>,<Address Type>,<Connection Type>, where
<Peer BT Address>– Is the 6-byte hex address of the peer device<Address Type>– Is either0for public address or1for random address<Connection Type>– Specifies if the connection enables the UART transparent feature, where1indicates UART transparent is enabled and0indicates UART transparent is disabled
- <Peer BT Address>,<Address Type>,<Connection Type>, where
| Example: | GK | // Get current connection status |
| Response: | None or Err | // If not connected |
<Peer BT Address>,<Address Type>,<Connection Type> | // If connected | |
GK,0071 | // Get the current connection status of the dedicated connected device for multiple links. <hex16> is the connection handle of the remote-dedicated device. |