5.2.4 Enter Command Mode ($$$)
Format: $$$
This command makes the RNBD350 module enter Command mode and display the command prompt. The device passes the characters as data, and enters the Command mode if it sees the $$$ sequence. If the Command mode guard bit is set using the SR command, the device checks if there are any bytes before or after the $$$ characters in a one-second window, the device does not enter Command mode and these bytes are passed through. For more details on the SR command, refer to Set Application Options (SR,<hex16>).
The user can change the character string used to enter the Command mode using the S$ command. For more details on the S$ command, refer to Set Enter Command Character (S$,<char>).
The UART receives a CMD> prompt indicating the start of a command session.
| Example: | $$$ | // Enter Command mode |
| Response: | CMD> | // If command prompt is enabled |