5.2.25 Set HCI Determination (SH,<0,1>)
Format: SH,<0,1>
This command is used to enable/disable the determining scheme to enter the HCI mode:
- 1: Enable HCI mode determining scheme
- 0: Disable HCI mode determining scheme
The determining scheme is to check the first command format to judge if the RNBD350 module is in HCI mode or RN application after reboot. When the RNBD350 module enters HCI mode, it will be recorded into PDS and invalidate the determining scheme. The GH command will navigate to the Get_Configuration.
| Example: | SH,1 | // Enable HCI mode determining scheme |
| Response: | AOK | // Success |
Err | // Syntax error or invalid parameter |
Note:
- The command is supported in RNBD350 v1.1 and later.
- The parameter of
SHcommand is stored in PDS.