Depending on the AFE selected, the metrology module generates the following
accumulated current (I2) quantities: CYCLE_I_A, CYCLE_I_B, CYCLE_I_C,
CYCLE_I_Nm, CYCLE_I_A_F, CYCLE_I_B_F, CYCLE_I_C_F, and CYCLE_I_Nm_F.
CYCLE_I_x, CYCLE_I_x_F
These accumulators are in units of [Amp2 samp scaled] in the [uQ24.40]
format and represent the accumulated scaled current in the last line cycle
measurement period. They are calculated according to the following formula:
Where,
- I_x_samplei is ith sampled current value of phase x
in the present cycle
- x = [A, B, C, A_F, B_F, C_F]
- N = The number of samples in the last cycle
CYCLE_I_Nm, CYCLE_I_Nm_F
These accumulators are in units of [Amp2 samp scaled] in the uQ24.40
format and represent the accumulated scaled neutral current in the last line cycle
measurement period. They are calculated according to the following formula:
Where,
- I_x_samplei is ith sampled neutral current value in
the present cycle
- x = [Nm, Nm_F]
- N = The number of samples in the last cycle
In the case of being multiplexed with temperature measurement acquisition, such as
when using the PIC32CXMTC with an external ATSENSE301, slightly less performance may
be expected than DSP-filtered full bandwidth data.