3.4 USB Connectivity
The WFI32E02 Module has an integrated USB peripheral that supports both low-speed and full-speed modes. This feature enables the user to implement USB functionality through the Micro-B USB connector (J207) on the PIC32 WFI32 Curiosity HPC Board. Connect the board using any one of these modes:
- Device mode:
- The user must power-up the PIC32 WFI32 Curiosity HPC Board using any of the two power sources before using the USB interface. For more details, refer to Power Supply.
- Connect the host PC to
the Micro-B USB connector (J207) using a male USB Type-A cable to Micro-B
male USB cable.Note: Do not place the jumper on the USB Host/Device mode selection header (J208).
- Host mode:
- The user must power-up the PIC32 WFI32 Curiosity HPC Board using any of the two power sources before using the USB interface. For more details, refer to Power Supply.
- Connect the USB device to the Micro-B USB connector (J207) using a female USB Type-A cable to Micro-B male USB cable.
- Place a jumper in the USB
Host/Device mode selection header (J208) to drive the VBUS line in the
Host mode.Note: USB Type-A cable to Micro-B male USB cable is not available in the PIC32 WFI32 Curiosity HPC Board kit.