The purpose of fastPollingMode is to continuously check all participating service/channel
configurations for valid telegrams without any interruption. This mode is very similar to the
PollingMode but there is no support of the self-check functionality and no sleep period is
executed, as shown in the following figure. Fast polling is also known as “scanning”.Figure 2-23. Fast Polling Cycle Definition
If the polling period is set to 0 ms in the confT1COR EEPROM setting, fastPollingMode is
activated. During operation, fastPollingMode can be enabled by overwriting the confT1COR SRAM
variable manually with 0x00 by using the “Write SRAM/Register” SPI command if the system is in
IDLEMode. For more information, see Write SRAM/Register.
Note: EOP signals are ignored in this mode.
Furthermore, VCO tuning on the initial service/channel configuration is not supported. For
more information, see VCO Tuning.