1.1.15.3 WDRV_WINC_SystemTimeSetCurrent Function
WDRV_WINC_STATUS WDRV_WINC_SystemTimeSetCurrent (
DRV_HANDLE handle, uint32_t curTime
)
C
Summary
Sets the current system time on the WINC.
Description
Configures the system time to the UTC value specified.
Precondition
WDRV_WINC_Initialize should have been called. WDRV_WINC_Open should have been called to obtain a valid handle.
Parameters
Param | Description |
handle | Client handle obtained by a call to WDRV_WINC_Open. |
curTime | The current UTC time (epoch 01/01/1970). |
Returns
WDRV_WINC_STATUS_OK - The request has been accepted. WDRV_WINC_STATUS_NOT_OPEN - The driver instance is not open. WDRV_WINC_STATUS_INVALID_ARG - The parameters were incorrect. WDRV_WINC_STATUS_REQUEST_ERROR - The request to the WINC was rejected.
Remarks
None.