1.1.2.4.4 DRV_G3_MACRT_TxRequest Function
C
void DRV_G3_MACRT_TxRequest (
const DRV_HANDLE handle,
uint8_t *pData,
uint16_t length
);Summary
Allows a client to transmit G3 MAC data through Power Line (PLC).
Description
This routine sends a new data message through PLC using the G3 MAC RT driver. The message must have a valid IEEE 802.15.4 MAC format with its corresponding MAC header.
Precondition
DRV_G3_MACRT_Open must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid instance handle, returned from the driver's open routine |
| pData | Pointer to the data to transmit |
| length | Length of the data to transmit in bytes |
Returns
None.
Example
// 'handle', returned from DRV_G3_MACRT_Open previously called
// Local function implemented in the user application
_setupTransmissionParameters();
DRV_G3_MACRT_TxRequest(handle, appData.pData, appData.length);Remarks
None.