1.1.2.4.10 DRV_G3_MACRT_DataIndCallbackRegister Function
C
void DRV_G3_MACRT_DataIndCallbackRegister (
const DRV_HANDLE handle,
const DRV_G3_MACRT_DATA_IND_CALLBACK callback
);Summary
Allows a client to set a G3 MAC RT data indication event handling function for the driver to call back when a data reception has finished.
Description
This function allows a client to register a G3 MAC RT data indication event handling function for the driver to call back when a data reception PLC event occurs.
Before this callback is set, any received frame by the PLC transceiver will not be notified. The callback once set, persists until the client closes the driver or sets another callback (which could be a NULL pointer to indicate no callback).
Precondition
DRV_G3_MACRT_Open must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid instance handle, returned from the driver's open routine |
| callback | Pointer to the callback function |
Returns
None.
Example
// Event is received when a frame is received void APP_PLC_Data_Ind_callback(uint8_t *pData, uint16_t length) { // Reception handling here. if (length) { memcpy(myAppObj->pDataRcv, pData, length); myAppObj->lengthDataRcv = length; } } // myAppObj is an application specific state data object. MY_APP_OBJ myAppObj; // Client registers a data indication callback with driver. This is done once // 'myHandle', returned from DRV_G3_MACRT_Open previously called DRV_G3_MACRT_DataIndCallbackRegister( myAppObj.myHandle, APP_PLC_Data_Ind_callback );
Remarks
None.