1.1.3.4.9 DRV_RF215_SetChannelCallbackRegister Function
C
void DRV_RF215_SetChannelCallbackRegister (
DRV_HANDLE drvHandle,
const DRV_RF215_SET_CHANNEL_CALLBACK callback,
uintptr_t context
);
Summary
Allows a client to set an event handling function for the driver to call back when frequency channel is updated.
Description
This function allows a client to register a an event handling function for the driver to call back when frequency channel is updated(confirmation of DRV_RF215_SetChannelRequest).
The callback should be registered immediately after opening the driver.
Precondition
DRV_RF215_Open must have been called to obtain a valid opened driver handle.
Parameters
| Param | Description |
|---|---|
| drvHandle | A valid open-instance handle, returned from the driver's open routine. |
| callback | Pointer to the callback function. |
| context | The value of this parameter will be passed back to the client unchanged, when the callback function is called. |
Returns
None.
Example
static void APP_SetChannelCb(DRV_RF215_TX_RESULT result, uintptr_t ctxt) { // The context handle was set to an application specific object // It is now retrievable easily in the event handler MY_APP_OBJ myAppObj = (MY_APP_OBJ *) ctxt; // Set channel handling here. } SYS_MODULE_OBJ sysObjDrvRf215; // Returned from DRV_RF215_Initialize SYS_STATUS drvRf215Status; DRV_HANDLE drvRf215Handle; MY_APP_OBJ myAppObj; // Application specific data object drvRf215Status = DRV_RF215_Status(sysObjDrvRf215); if (drvRf215Status == SYS_STATUS_READY) { // This means now the driver can be opened using DRV_RF215_Open routine drvRf215Handle = DRV_RF215_Open(DRV_RF215_INDEX_0, RF215_TRX_ID_RF09); if (drvRf215Handle != DRV_HANDLE_INVALID) { // Driver opened successfully. Register callback DRV_RF215_SetChannelCallbackRegister(drvRf215Handle, APP_SetChannelCb, (uintptr_t) myAppObj); } }
Remarks
The callback once set, persists until the client closes the driver or sets another callback (which could be a NULL pointer to indicate no callback).
This function is only available if "Frequency hopping support" is enabled through MCC.