1.1.3.4.6 DRV_RF215_Close Function
C
void DRV_RF215_Close( const DRV_HANDLE drvHandle );
Summary
Closes an opened-instance of the RF215 driver.
Description
This routine closes an opened-instance of the RF215 driver, invalidating the handle. A new handle must be obtained by calling DRV_RF215_Open before the caller may use the driver again.
Precondition
DRV_RF215_Open must have been called to obtain a valid opened driver handle.
Parameters
| Param | Description |
|---|---|
| drvHandle | A valid open-instance handle, returned from the driver's open routine. |
Returns
None.
Example
// 'drvHandle', returned from DRV_RF215_Open DRV_RF215_Close(drvHandle);
Remarks
None.