3.4.12.1 Import the Microchip HSM Public Verify Key
Once the customer receives the Microchip HSM public verify key, they need to import it into the
U-HSM. Use the U‑HSMGenImp utility for this type of import:
pkg-g4mf-seespk-<hex>: This is the file on the disk with
the key to be imported for verifying signature.
For example: pkg-g4mf-seespk-121187e7
The resulting files are created in the Security World key folder. Information about these keys can be viewed using the nfkminfo -k command.
Example of the resulting key file:
key_simple_g4mf-seespk