1.44 CRYPT_TDES_IvSet Function
C
int CRYPT_TDES_IvSet(
CRYPT_TDES_CTX* tdes,
const unsigned char* iv
);
Description
This function changes the initialization vector (IV) of a TDES context, but leaves the key alone.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| tdes | Pointer to context which saves state between calls. |
| iv | Pointer to buffer holding the initialization vector. Must be 8 bytes in size. |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function.
- 0 - An invalid pointer was not passed to the function.
Remarks
The IV must be 8 bytes long.
Example
CRYPT_TDES_CTX mcDes3;
int ret;
byte out1[TDES_SIZE];
byte out2[TDES_SIZE];
strncpy((char*)key, "1234567890abcdefghijklmn", 24);
strncpy((char*)iv, "12345678", 8);
ret = CRYPT_TDES_KeySet(&mcDes3, key, iv, CRYPT_TDES_ENCRYPTION);
ret = CRYPT_TDES_IvSet(&mcDes3, iv);
ret = CRYPT_TDES_CBC_Encrypt(&mcDes3, out1, ourData, TDES_SIZE);
ret = CRYPT_TDES_KeySet(&mcDes3, key, iv, CRYPT_TDES_DECRYPTION);
ret = CRYPT_TDES_CBC_Decrypt(&mcDes3, out2, out1, TDES_TEST_SIZE);