1.35 CRYPT_RSA_Free Function
C
int CRYPT_RSA_Free(
CRYPT_RSA_CTX* rsa
);
Description
This function releases the memory used during RSA processing for storing the public/private key.
Preconditions
The context must have been set up previously with a call to CRYPT_RSA_Initialize.
Parameters
| Parameters | Description |
|---|---|
| rsa | Pointer to context to clean up. |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function.
- 0 - An invalid pointer was not passed to the function.
Remarks
None.
Example
CRYPT_RSA_CTX mcRsa;
int ret;
ret = CRYPT_RSA_Initialize(&mcRsa);
ret = CRYPT_RSA_Free(&mcRsa);