1.31 CRYPT_ECC_PublicImport Function
C
int CRYPT_ECC_PublicImport(
CRYPT_ECC_CTX* ecc,
const unsigned char* in,
unsigned int inSz
);
Description
This function imports a public key in ANSI X9.63 format into the ECC context.
Preconditions
The ECC context must have previously been initialized with a call to CRYPT_ECC_Initialize.
Parameters
| Parameters | Description |
|---|---|
| ecc | Pointer to context which saves state between calls. |
| in | Input buffer that holds the public key. |
| inSz | Size of the input buffer, in bytes. |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function.
- MEMORY_E - Memory could not be allocated for the key.
- ASN_PARSE_E - There was a parse error while going through the key.
- 0 - An invalid ppointer was not passed to the function.
Remarks
None.
Example
CRYPT_ECC_CTX userB;
int ret;
byte sharedA[100];
unsigned int aSz = (unsigned int)sizeof(sharedA);
unsigned int usedA;
ret = CRYPT_ECC_Initialize(&userB);
...
ret = CRYPT_ECC_PublicImport(&userB, sharedA, usedA);