1.34 CRYPT_RSA_EncryptSizeGet Function
C
int CRYPT_RSA_EncryptSizeGet(
CRYPT_RSA_CTX* rsa
);
Description
This function retrieves the size of the RSA key in use for the context.
Preconditions
The context must be initialized with a call to CRYPT_RSA_Initialize and the keys decoded either with CRYPT_RSA_PrivateKeyDecode or CRYPT_RSA_PublicKeyDecode.
Parameters
| Parameters | Description |
|---|---|
| rsa | Pointer to context which saves state between calls. |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function.
- int - Size of the key.
Remarks
None.
Example
CRYPT_RSA_CTX mcRsa;
int ret;
unsigned int keySz = (unsigned int)sizeof(client_key_der_1024);
byte out1[256];
ret = CRYPT_RSA_Initialize(&mcRsa);
ret = CRYPT_RSA_PrivateKeyDecode(&mcRsa, client_key_der_1024, keySz);
ret = CRYPT_RSA_EncryptSizeGet(&mcRsa);