1.32 CRYPT_ECC_SignatureSizeGet Function
C
int CRYPT_ECC_SignatureSizeGet(
CRYPT_ECC_CTX* ecc
);
Description
This function returns the size of the signature in a given context, in octets.
Preconditions
The ECC context must have been initialized with a call to CRYPT_ECC_Initialize. The keys must have been imported or created prior to calling this function.
Parameters
| Parameters | Description |
|---|---|
| ecc | Pointer to context which saves state between calls, and contains the signature. |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function.
- int - The size of the signature.
Remarks
None.
Example
CRYPT_ECC_CTX userA;
int ret;
byte sig[100];
unsigned int sigSz = (unsigned int)sizeof(sig);
unsigned int usedA = 0;
ret = CRYPT_ECC_Initialize(&userA);
...
// Import or generate private key
...
ret = CRYPT_ECC_SignatureSizeGet(&userA);