1.28 CRYPT_ECC_KeySizeGet Function
C
int CRYPT_ECC_KeySizeGet(
CRYPT_ECC_CTX* ecc
);
Description
This function returns the size of the ECC key, in octets.
Preconditions
The ECC context must have been initialized with a call to CRYPT_ECC_Initialize. The key must have been imported or created prior to calling this function.
Parameters
| Parameters | Description |
|---|---|
| ecc | Pointer to context which saves state between calls and contains the key. |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function.
- int - The size of the key, in octets.
Remarks
None.
Example
CRYPT_ECC_CTX userA;
int ret;
byte sig[100];
unsigned int sigSz = (unsigned int)sizeof(sig);
unsigned int usedA = 0;
ret = CRYPT_ECC_Initialize(&userA);
...
// Import or generate private key
...
ret = CRYPT_ECC_KeySizeGet(&userA);