1.27 CRYPT_ECC_Initialize Function
C
int CRYPT_ECC_Initialize(
CRYPT_ECC_CTX* ecc
);
Description
This function initializes the context used for Elliptic Curve Cryptography (ECC). The context is then passed to calls to perform key building, encryption, decryption, etc.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| ecc | Pointer to context to initialize. |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function.
- -1 - Unable to allocate memory for the keys.
- 0 - An invalid pointer was not passed to the function.
Remarks
None.
Example
CRYPT_ECC_CTX userA;
int ret;
ret = CRYPT_ECC_Initialize(&userA);