1.56 CRYPT_SHA224_Finalize Function
C
int CRYPT_SHA224_Finalize(
CRYPT_SHA256_CTX* sha224,
unsigned char* digest
);
Description
This function finalizes the hash and puts the result into digest.
Preconditions
The SHA224 context must be initialized prior to calling this function. The context must not be modified by code outisde of this function.
Parameters
| Parameters | Description |
|---|---|
| sha224 | Pointer to CRYPT_SHA256_CTX structure which holds the hash values. |
| digest | Pointer to byte array to store hash result. |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function, either sha224 or digest.
- 0 - An invalid pointer was not passed to the function.
Remarks
In order to preserve the validity of the SHA224 hash, nothing must modify the context holding variable between calls to CRYPT_SHA224_DataAdd and CRYPT_SHA224_Finalize.
Example
CRYPT_SHA256_CTX sha224;
uint8_t buffer[1024];
uint8_t shaSum[SHA224_DIGEST_SIZE];
CRYPT_SHA224_Initialize(&sha224);
CRYPT_SHA224_DataAdd(&sha224, buffer, sizeof(buffer));
CRYPT_SHA224_Finalize(&sha224, shaSum);