1.17 CRYPT_AES_GCM_Encrypt Function
C
int CRYPT_AES_GCM_Encrypt(
CRYPT_AES_CTX* aes,
unsigned char* out,
const unsigned char* in,
unsigned int sz,
const unsigned char* iv,
unsigned int ivSz,
unsigned char* authTag,
unsigned int authTagSz,
const unsigned char* authIn,
unsigned int authInSz
);
Description
This function encrypts a block of data using the AES algorithm in Galois/Counter Mode (GCM).
Preconditions
Key must be set earlier with a call to CRYPT_AES_GCM_SetKey.
Parameters
| Parameters | Description |
|---|---|
| aes | Pointer to context which saves state between calls. |
| out | Pointer to buffer to store the results of the encryption pass. |
| in | Pointer to buffer holding the data to be encrypted. |
| sz | Size of the input data, in bytes. |
| iv | Pointer to the initialization vector. |
| ivSz | Size of the initialization vector. |
| authTag | Pointer to the buffer to store the authentication tag. |
| authTagSz | Size of the authentication tag. |
| authIn | Pointer to the additional authentication data. |
| authInSz | Size of the additional authentication data. |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function.
- 0 - An invalid pointer was not passed to the function.
Remarks
The output buffer must be equal in size to the input buffer.