1.40 CRYPT_RSA_PublicKeyDecode Function
C
int CRYPT_RSA_PublicKeyDecode(
CRYPT_RSA_CTX* rsa,
const unsigned char* in,
unsigned int inSz
);
Description
This function builds a public key from a DER-formatted certificate. DER stands for Distinguished Encoding Rules.
Preconditions
The context must have been initialized with a call to CRYPT_RSA_Initialize.
Parameters
| Parameters | Description |
|---|---|
| rsa | Pointer to context which saves state between calls. |
| in | Pointer to buffer containing the certificate to process to extract the public key. |
| inSz | Size of the input data in bytes. |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function.
- 0 - An invalid pointer was not passed to the function.
Remarks
None.
Example
CRYPT_RSA_CTX mcRsa;
int ret;
unsigned int keySz = (unsigned int)sizeof(client_key_der_1024);
ret = CRYPT_RSA_Initialize(&mcRsa);
ret = CRYPT_RSA_PublicKeyDecode(&mcRsa, client_key_der_1024, keySz);
ret = CRYPT_RSA_PublicEncrypt(&mcRsa, out1, sizeof(out1), ourData, RSA_TEST_SIZE, &mcRng);