1.37 CRYPT_RSA_PrivateDecrypt Function
C
int CRYPT_RSA_PrivateDecrypt(
CRYPT_RSA_CTX* rsa,
unsigned char* out,
unsigned int outSz,
const unsigned char* in,
unsigned int inSz
);
Description
This function decrypts a data block using a private key.
Preconditions
The context must be initialized using CRYPT_RSA_Initialize and the private key decoded using CRYPT_RSA_PrivateKeyDecode prior to calling this function.
Parameters
| Parameters | Description |
|---|---|
| rsa | Pointer to context which saves state between calls. |
| out | Pointer to output buffer to store results. |
| outSz | Size of output buffer. |
| in | Pointer to source buffer to be decrypted. |
| inSz | Size of input buffer. |
Returns
- BAD_FUNC_ARG - An invalid pointer was passed to the function.
- int - Size of the actual output.
Remarks
None.
Example
CRYPT_RSA_CTX mcRsa;
int ret;
unsigned int keySz = (unsigned int)sizeof(client_key_der_1024);
byte out1[256];
ret = CRYPT_RSA_Initialize(&mcRsa);
ret = CRYPT_RSA_PrivateKeyDecode(&mcRsa, client_key_der_1024, keySz);
ret = CRYPT_RSA_PrivateDecrypt(&mcRsa, out2, sizeof(out2), out1, RSA_TEST_SIZE);