2.3.3.2.6 Use Content for Simulation
(Ask a Question)Select to include the memory content for simulation. When this checked, a
UPROM.mem file is automatically created in the
<prj_location>/simulation folder when simulation is invoked in
the Design Flow window. The UPROM.mem file is read by the μPROM simulation
model to initialize the μPROM content when the simulation starts. Only clients with the
Use Client for Simulation check box checked have the contents added to the
UPROM.mem file for simulation.
The following figure shows the added clients under User clients in μPROM.