The revision history table describes the changes that were implemented in
the document. The changes are listed by revision, starting with the most current
publication.
Table 7-1. Revision History| Revision | Date | Description |
|---|
| H | 05/2025 | The following is the summary of changes in this revision of the
document: |
| G | 09/2023 | The following is the summary of changes in this revision of the
document: |
| F | 03/2023 | The following is the summary of changes in this revision of the
document:- Updated the document
title and added RT PolarFire information.
- In μPROM, modified the
sentence to mention that fabric logic has read-only access to µPROM.
- Updated ECC Mode (For x33 Two-Port Mode Only) to include information about Multi-bit errors.
|
| E | 07/2022 | The following is the summary of changes in this revision of the
document: |
| D | 03/2022 |
The following is the summary of changes in this revision of the
document:
|
| C | 12/2021 | The following is the summary of changes in this revision of the
document: |
| B | 08/2021 | Added MPF for PolarFire FPGA and MPFS for PolarFire SoC FPGA in Introduction. |
| A | 08/2021 |
The first publication of this document. This user guide was created by
merging the following documents:
- UG0680: PolarFire FPGA
Fabric User Guide
- UG0912: PolarFire SoC
FPGA Fabric User Guide
For more information, see Table 7-2
and Table 7-3 respectively.
|
The following revision history table describes the changes that were implemented in the
UG0680: PolarFire FPGA Fabric User Guide document. The changes are listed by revision.
Note: UG0680: PolarFire FPGA Fabric User Guide
document is now obsolete and the information in the document has been migrated to
PolarFire® FPGA and PolarFire SoC FPGA Fabric User Guide.
Table 7-2. Revision History of UG0680: PolarFire FPGA Fabric User Guide| Revision | Date | Description |
|---|
| Revision 7.0 | 04/2021 |
- Updated the Read
Operation in Dual-Port Mode figure to correct the output data
values in the Pipeline Mode.
- Removed collision
prevention from the LSRAM, μSRAM, μPROM, and sNVM Features
table.
- Updated the Byte Write
Enables Settings for Dual-Port Mode table 8 for 1K x 16 mode.
- Added information about
how RAM blocks are cascaded when Write byte Enables option is
selected.
- Updated μPROM Operation
to mention that μPROM memory file supports only the plain text file.
- Updated the Simplified
Functional Block Diagram of LSRAM in Dual-Port Mode figure and
Simplified Functional Block Diagram for LSRAM in Two-Port Mode
figure to show that A_BYPASS and B_BYPASS signals are control signals of
the MUX.
- Removed Simple Write,
Feed-Through Write, and Read-Before-Write specific content from two-port
LSRAM. These write operations are not supported in the two-port LSRAM
configuration.
|
| Revision 6.0 | 04/2020 | Updated information for for x33 Two-Port Mode Only in ECC mode. |
| Revision 5.0 | 04/2019 |
- Structural changes were
made throughout the document.
- Information about
PolarFire LSRAM, μSRAM, μPROM, and sNVM Features were updated in the
LSRAM, μSRAM, μPROM, and sNVM Features table.
- Math Block Features were
updated.
- Libero SoC PolarFire
Compile Report is moved to appendix.
|
| Revision 4.0 | 03/2018 | Updated the Math Blocks Resources in the Fabric Resources in PolarFire
Family table. |
| Revision 3.0 | 11/2017 | Revision 3.0 of this document is updated to include features and
enhancements introduced in Libero SoC PolarFire v2.0. |
| Revision 2.0 | 06/2017 |
- Added reference to the
ChipPlanner user guide.
- Added reference to the
Synplify Pro RAM block application note for LSRAM.
- Added reference to the
Synplify Pro RAM block application note for μSRAM.
- Added reference to the
Synplify Pro MACC block application note for MACC.
|
| Revision 1.0 | 02/2017 | The first publication of the document. |
The following revision history table describes the changes that were implemented in the
UG0912: PolarFire SoC FPGA Fabric User Guide document. The changes are listed by
revision.
Note: UG0912: PolarFire SoC FPGA Fabric User
Guide document is now obsolete and the information in the document has been migrated to
PolarFire® FPGA and PolarFire SoC FPGA Fabric User Guide.
Table 7-3. Revision History of UG0912: PolarFire SoC FPGA Fabric User Guide| Revision | Date | Description |
|---|
| Revision 2.0 | 04/2021 |
- Updated the Read Operation in Dual-Port Mode figure to correct
the output data values in the Pipeline Mode.
- Removed collision prevention from the Memory Blocks table.
- Updated the Byte Write Enables Settings for Dual-Port Mode table
for 1K x 16 mode.
- Added information about how RAM blocks are cascaded when Write byte
Enables option is selected.
- Updated μPROM Operation to mention that μPROM memory file supports only
the plain text file.
- Updated the Simplified Functional Block Diagram of LSRAM in Dual-Port
Mode figure and Simplified Functional Block Diagram for LSRAM
in Two-Port Mode the figure to show that A_BYPASS and B_BYPASS
signals are control signals of the MUX.
- Removed Simple Write, Feed-Through Write, and Read-Before-Write specific
content from two-port LSRAM. These write operations are not supported in
the two-port LSRAM configuration.
|
| Revision 1.0 | 04/2020 | The first publication of the document. |