17.1.9.1.1 Working with derive_constraints Utility
(Ask a Question)Derive constraints traverse through the design and allocate new constraints for each instance of component based on previously provided component SDC files. For the CCC reference clocks, it propagates back through the design to find the source of the reference clock. If the source is an I/O, the reference clock constraint will be set on the I/O. If it is a CCC output or another clock source (for example, Transceiver, oscillator), it uses the clock from the other component and reports a warning if the intervals do not match. Derive constraints will also allocate constraints for some macros like on-chip oscillators if you have them in your RTL.
To execute the derive_constraints
utility, you must supply a
.tcl file command-line argument with the following information
in the specified order.
- Specify device information using the information in section 17.1.9.1.2 set_device.
- Specify path to the RTL files using the information in section 17.1.9.1.3 read_verilog or 17.1.9.1.4 read_vhdl.
- Set top level module using the information in section 17.1.9.1.5 set_top_level.
- Specify path to the component SDC files using the information in section 17.1.9.1.6 read_sdc or 17.1.9.1.7 read_ndc.
- Execute the files using the information in section 17.1.9.1.8 derive_constraints.
- Specify path to the SDC derived constraints file using the information in section 17.1.9.1.9 write_sdc or 17.1.9.1.10 write_pdc or 17.1.9.1.11 write_ndc.
Execution and Contents of the derive.tcl File
The following is an example command-line argument to execute the
derive_constraints
utility.
$ <libero_installation_path>/bin{64}/derive_constraints derive.tcl
The contents of the derive.tcl file:
# Device information set_device -family PolarFire -die MPF100T -speed -1 # RTL files read_verilog -mode system_verilog project/component/work/txpll0/txpll0_txpll0_0_PF_TX_PLL.v read_verilog -mode system_verilog {project/component/work/txpll0/txpll0.v} read_verilog -mode system_verilog {project/component/work/xcvr0/I_XCVR/xcvr0_I_XCVR_PF_XCVR.v} read_verilog -mode system_verilog {project/component/work/xcvr0/xcvr0.v} read_vhdl -mode vhdl_2008 {project/hdl/xcvr1.vhd} #Component SDC files set_top_level {xcvr1} read_sdc -component {project/component/work/txpll0/txpll0_0/txpll0_txpll0_0_PF_TX_PLL.sdc} read_sdc -component {project/component/work/xcvr0/I_XCVR/xcvr0_I_XCVR_PF_XCVR.sdc} #Use derive_constraint command derive_constraints #SDC/PDC/NDC result files write_sdc {project/constraint/xcvr1_derived_constraints.sdc} write_pdc {project/constraint/fp/xcvr1_derived_constraints.pdc}