21.11.9 export_script

Description

This Tcl command explicitly exports the Tcl command equivalents of the current FlashPro Express session. With this command you can re-execute the same commands interactively or in batch.

You must supply a file name with the -file parameter and the -relative_path parameter to specify whether an absolute or relative path is used in the exported script file.

export_script \
-file {absolute or relative path to exported file} \
-relative_path <value>

Arguments

ParameterTypeDescription

file

string

Specifies the absolute or relative path and name for the exported TCL script.

relative_path

boolean

Sets your option to use a relative or absolute path in the exported script; use 1 for relative path, 0 for absolute path.

Return TypeDescription
NoneNone

Error Codes

Error CodeDescription

None

Parameter 'file' has illegal value.

None

Required parameter 'relative_path' is missing.

Supported Families

PolarFire®
SmartFusion® 2

Example

The following command exports the Tcl command equivalents of the current FlashPro Express session in exported.tcl:

export_script -file {./exported.tcl} -relative_path 1