Description
This Tcl command updates all the FlashPro6 programmers that require update. This
command takes no parameters. To execute the Tcl Command in Libero SoC, add the
command before run_tool
. To execute the Tcl command in FlashPro
Express tool or SmartDebug tool, add the Tcl command before
run_selected_actions
.
update_fp6_programmers
Arguments
Parameter |
Type |
Description |
None |
None |
None |
Return Type |
Description |
None |
None |
Error Codes
Error Code |
Description |
None |
Parameter 'param_name' is not defined. Valid command formatting
is 'update_fp6_programmers'. |
Example
This example updates all the FlashPro6 programmers that require update.
update_fp6_programmers