21.14.5 sb_move_core
(Ask a Question)Description
A Fabric AMBA Master configured as AXI or AHBLite can be added to the Fabric DDR Subsystem to enable a fabric master to access external DDR memory using FDDR. Alternatively, the Fabric DDR RAM can also be moved (drag and drop) to other Subsystems in the Peripherals page so that the master(s) in that Subsystem will also be able to access external DDR memory using FDDR.
For example, the
                        Fabric_DDR_RAM can be moved from its default 'Fabric DDR Subsystem' to 'MSS
                        FIC_0 - MSS Master Subsystem' (FIC0_Master_Subsystem) which will enable
                        Cortex-M3 in the MSS to access external DDR memory using FDDR via FIC_0
                        Master address space.  The Tcl command sb_move_core will be
                        used to capture the action of moving the Fabric_DDR_RAM to a different
                        Subsystem in the exported Tcl description for a System Builder
                        component.
sb_move_core \
-component_name {component_name} \
[-core_name {core_name}] \
-subsystem_name {subsystem_name}
        Arguments
| Parameter | Type | Description | 
|---|---|---|
| -component_name {component_name} | string | Mandatory. Name of the system builder component. | 
| -core_name {core_name} | string | Optional. Name of the instance of the core in the System Builder component. | 
| -subsystem_name {subsystem_name} | string | Mandatory. Name of the subsystem the core is being added to. | 
Example
sb_move_core -component_name {sb} -core_name {Fabric_DDR_RAM} -subsystem_name {FIC0_Master_Subsystem}