8.2 Fold Instance
(Ask a Question)The expanded hierarchy of an instance can be folded or collapsed back into the parent instance.
Use one of the following three ways to fold/collapse the expanded instance back into the parent instance:
- Click the - button at the
top left of the instance.
Figure 8-34. Fold Instance Icon - Click to select the expanded instance, then right click and select Fold
Instance in the menu.
Figure 8-35. Fold Instance Menu Item - Click the Fold All Instance icon.