8.2 Expand InPlace
(Ask a Question)Use one of the following two ways to execute the Expand Inplace operation on an instance.
- Click the + button at the top left of the instance, which indicates that it is pushable.
- Left click to select the instance and then right click to select Expand Inplace.