9.12.8 PDC Setting
(Ask a Question)A PDC file is not needed for these I/Os because the settings from the MSS Configurator are being used. If the user specifies a correct placement and I/O standard, the tool will accept the user’s settings and will not error-out. But if the user tries to set any of the other specific MSS I/O attributes, it will fail. These constraints will not be written in the generated PDC file from the Chip Planner.