IPV6_EVENT_TYPE Enumeration
C
typedef enum {
IPV6_EVENT_ADDRESS_ADDED = 1,
IPV6_EVENT_ADDRESS_REMOVED,
IPV6_EVENT_ULA_ADDRESS_GENERATED,
IPV6_EVENT_ULA_ADDRESS_FAILED
} IPV6_EVENT_TYPE;
Description
Enumeration: IPV6_EVENT_TYPE.
These events are used while notifying to the registered applications.
Members
| Members | Description |
|---|---|
| IPV6_EVENT_ADDRESS_ADDED = 1 | Event is generated when IPv6 added to the list. |
| IPV6_EVENT_ADDRESS_REMOVED | Event is generated when IPv6 address removed from the list. |
| IPV6_EVENT_ULA_ADDRESS_GENERATED | Event is generated when IPv6 unique local address included to the list. |
| IPV6_EVENT_ULA_ADDRESS_FAILED | Event is generated when IPv6 unique local address is failed. |
Remarks
None.