TCPIP_IPV6_SourceAddressGet Function
C
IPV6_ADDR * TCPIP_IPV6_SourceAddressGet(
IPV6_PACKET * p
);
Description
This API is used to get the source address for an IPv6 packet.
Preconditions
TCPIP_IPV6_Initialize() is required. TCPIP_IPV6_InterfaceIsReady should be true.
Parameters
| Parameters | Description |
|---|---|
| p | Pointer to IPv6 packet. |
Returns
IPV6_ADDR *
Get a valid IPv6 Source address - On Success.
NULL - On Failure.
Remarks
None.