TCPIP_IPV6_UnicastAddressAdd Function
C
IPV6_ADDR_STRUCT * TCPIP_IPV6_UnicastAddressAdd(
TCPIP_NET_HANDLE netH,
IPV6_ADDR * address,
int prefixLen,
uint8_t skipProcessing
);
Description
Adds a unicast address to a specified interface. Starts duplicate address detection if necessary.
Preconditions
TCPIP_IPV6_Initialize() is required. TCPIP_IPV6_InterfaceIsReady should be true.
Parameters
| Parameters | Description |
|---|---|
| netH | The interface to which the address is to be added. |
| address | The address to add. |
| prefixLen | The prefix length associated to this static address (providing the subnet prefix length). If 0, the default value of 64 will be used. |
| skipProcessing | True to skip duplicate address detection; otherwise, false. |
Returns
IPV6_ADDR_STRUCT *
On Success - Pointer to the structure of the newly allocated address.
On Failure - NULL.
Remarks
The RFC (4291) requires the interface ID for all unicast addresses, (except those that start with the binary value 000) to be 64 bits long and to be constructed in Modified EUI-64 format. Therefore the prefixLen parameter should probably always be 64.