IPV6_PACKET_ACK_FNC Type
C
typedef bool (* IPV6_PACKET_ACK_FNC)(void*, bool, const void*);
Description
Type: IPV6_PACKET_ACK_FNC.
Packet allocation and deallocation acknowledgment callback function.
Parameters
| Parameters | Description |
|---|---|
| void * | Pointer to the packet that was transmitted. |
| bool | True if the packet was sent, False otherwise. |
| const void* | 0. |
Returns
True - If the packet needs the queuing flags removed (it is not deleted and still in use).
False - If the packet does not need the queuing flags removed (either no longer exists or the flags updated).
Remarks
None.