TCPIP_IPV6_MaxDatagramDataSizeGet Function
C
int TCPIP_IPV6_MaxDatagramDataSizeGet(
TCPIP_NET_HANDLE netH
);
Description
This function is a helper to allow retrieving the MDDS on the specified interface.
Preconditions
TCPIP_IPV6_Initialize() should be called. TCPIP_IPV6_InterfaceIsReady should be true.
Parameters
| Parameters | Description |
|---|---|
| netH | Handle of the interface. |
Returns
The maximum datagram data size that can be transported on the selected interface.
0 - Invalid interface specified.
Remarks
None.