TCPIP_IPV6_PutArray Macro
C
#define TCPIP_IPV6_PutArray(pkt,data,len) TCPIP_IPV6_ArrayPutHelper(pkt, data, IPV6_DATA_PIC_RAM, len)
Description
This function writes data to an outgoing packet.
Preconditions
TCPIP_IPV6_Initialize() is required. TCPIP_IPV6_InterfaceIsReady should be true. The TCPIP_IPV6_TxIsPutReady() function must have returned a value greater than or equal to len.
Members
| Members | Description |
|---|---|
| ptrPacket | The packet. |
| dataSource | Pointer to the data to copy to the packet. |
| len | Length of the data. |
Returns
unsigned short - The number of bytes of data written.
Remarks
None.