| Functions | |
| TCPIP_IPV6_HandlerRegister | Registers an IPv6 event handler callback function. |
| TCPIP_IPV6_HandlerDeregister | Deregisters an IPv6 event handler callback function. |
| TCPIP_IPV6_InterfaceIsReady | Determines if an interface is ready for IPv6 transactions. |
| TCPIP_IPV6_PacketFree | Frees a TCP/IP Packet structure from dynamic memory. |
| TCPIP_IPV6_PayloadSet | Allocates a segment on the end of a packet segment chain and uses it to address prebuffered data. |
| TCPIP_IPV6_DASSourceAddressSelect | Determines the appropriate source address for a given destination address. |
| TCPIP_IPV6_DestAddressGet | Gets the destination address for a IPv6 packet. |
| TCPIP_IPV6_DestAddressSet | Sets the destination address for a IPv6 packet. |
| TCPIP_IPV6_SourceAddressGet | Gets the source address for an IPv6 packet. |
| TCPIP_IPV6_SourceAddressSet | Sets the source address for a IPv6 packet. |
| TCPIP_IPV6_ArrayPutHelper | Helper function to write data to a packet. |
| TCPIP_IPV6_Put | Writes a character of data to a packet. |
| TCPIP_IPV6_TxIsPutReady | Determines whether a TX packet can be written to. |
| TCPIP_IPV6_TxPacketAllocate | Dynamically allocates a packet for transmitting IP protocol data. |
| TCPIP_IPV6_ArrayGet | Reads the next byte of data from the specified MAC. |
| TCPIP_IPV6_Flush | Flushes a IP TX packet. |
| TCPIP_IPV6_Get | Reads the next byte of data from the specified MAC. |
| TCPIP_IPV6_UniqueLocalUnicastAddressAdd | Adds a Unique Local Unicast Address (ULA) to a specified interface. |
| TCPIP_IPV6_RouterAddressAdd | Adds a new router address to a specified interface. |
| TCPIP_IPV6_UnicastAddressAdd | Adds a unicast address to a specified interface |
| TCPIP_IPV6_DefaultRouterDelete | Deletes the current router list for a specified interface |
| TCPIP_IPV6_DefaultRouterGet | Returns the current router address for a specified interface. |
| TCPIP_IPV6_Task | Standard TCP/IP stack module task function. |
| TCPIP_IPV6_IsFragmentationEnabled | Helper to get the IPv6 fragmentation support. |
| TCPIP_IPV6_MaxDatagramDataSizeGet | Helper to get the maximum datagream data size (MDDS) on a specific interface. |
| TCPIP_IPV6_AddressUnicastRemove | Removed a configured unicast address from an interface. |
| TCPIP_IPV6_MulticastListenerAdd | Adds a multicast listener to an interface. |
| TCPIP_IPV6_MulticastListenerRemove | Removes a multicast listener from a given interface. |
| TCPIP_IPV6_PacketHandlerDeregister | Deregisters a previously registered packet handler. |
| TCPIP_IPV6_PacketHandlerRegister | Sets a new packet processing handler. |
| Data Types and Constants | |
| IPV6_DATA_SEGMENT_HEADER | Data structure for IPv6 Data Segment header. |
| IPV6_NEXT_HEADER_TYPE | Defines a list of IPv6 next header types. |
| IPV6_PACKET | Packet structure/state tracking for IPv6 packets. |
| IPV6_PACKET_ACK_FNC | Packet allocation and deallocation acknowledgment callback function. |
| IPV6_SEGMENT_TYPE | Provides an enumeration of IPv6 segment types. |
| IPV6_ULA_FLAGS | Provides a list of possible ULA action flags. |
| IPV6_ULA_RESULT | Provides a list of possible ULA results. |
| IPV6_DATA_DYNAMIC_BUFFER | Data to transmit is allocated in dynamically allocated RAM |
| IPV6_DATA_NETWORK_FIFO | Data to transmit is stored in the Network Controller's FIFOs |
| IPV6_DATA_NONE | The data segment is unused |
| IPV6_DATA_PIC_RAM | Data to transmit is stored in PIC RAM |
| IPV6_NO_UPPER_LAYER_CHECKSUM | Value flag for no upper layer checksum |
| TCPIP_IPV6_PutArray | Writes data to a packet |
| _IPV6_DATA_SEGMENT_HEADER | Data structure for IPv6 Data Segment header. |
| _IPV6_PACKET | Packet structure/state tracking for IPv6 packets. |
| _IPV6_RX_FRAGMENT_BUFFER | Data structure for IPv6 Received fragmented packet. |
| TCPIP_IPV6_MODULE_CONFIG | Provides a place holder for IPv6 configuration. |
| IPV6_HEADER_OFFSET_DEST_ADDR | Header offset for destination address |
| IPV6_HEADER_OFFSET_NEXT_HEADER | Header offset for next header |
| IPV6_HEADER_OFFSET_PAYLOAD_LENGTH | Header offset for payload length |
| IPV6_HEADER_OFFSET_SOURCE_ADDR | Header offset for source address |
| IPV6_TLV_HBHO_PAYLOAD_JUMBOGRAM | IPv6 Type-length-value type code for the Hop-by-hop "Jumbo-gram Payload" option |
| IPV6_TLV_HBHO_ROUTER_ALERT | IPv6 Type-length-value type code for the Hop-by-hop "Router Alert" option |
| IPV6_TLV_PAD_1 | IPv6 Type-length-value type code for the Pad 1 option |
| IPV6_TLV_PAD_N | IPv6 Type-length-value type code for the Pad N option |
| IPV6_TLV_UNREC_OPT_DISCARD_PP | IPv6 action code for the unrecognized option reaction to discard the packet and send an ICMP parameter problem message |
| IPV6_TLV_UNREC_OPT_DISCARD_PP_NOT_MC | IPv6 action code for the unrecognized option reaction to discard the packet and send an ICMP parameter problem message is the destination address isn't a multicast address |
| IPV6_TLV_UNREC_OPT_DISCARD_SILENT | IPv6 action code for the unrecognized option reaction to discard the packet silently |
| IPV6_TLV_UNREC_OPT_SKIP_OPTION | IPv6 action code for the unrecognized option reaction to skip the option |
| IPV6_RX_FRAGMENT_BUFFER | Data structure for IPv6 Received fragmented packet. |
| IPV6_TLV_OPTION_TYPE | Data structure for IPv6 TLV options. |
| IPV6_HANDLE | Pointer to IPv6 object |
| IPV6_EVENT_TYPE | This enumeration is used to notify IPv6 client applications. |
| IPV6_EVENT_HANDLER | Clients can register a handler with the IPv6 service. |
| IPV6_ADDRESS_TYPE | Data structure for IPv6 address types. |
| IPV6_ADDRESS_PREFERENCE | Provides selection of public versus temporary addresses. |
| IPV6_ADDRESS_POLICY | Data structure for IPv6 address policy. |
| IPV6_ACTION | Provides a list of possible IPv6 actions. |
| TCPIP_IPV6_PACKET_HANDLER | Pointer to a function(handler) that will get called to process an incoming IPv6 packet. |
| TCPIP_IPV6_PROCESS_HANDLE | Defines a IPv6 packet processing handle. |