TCPIP_DNS_IsEnabled Function
C
bool TCPIP_DNS_IsEnabled(
TCPIP_NET_HANDLE hNet
);
Description
This function returns the current state of DNS Client on the specified interface.
Preconditions
The DNS module must be initialized.
Paramaters
Parameters | Description |
---|---|
hNet | Interface to query. |
Returns
True - If the DNS client service is enabled on the specified interface.
False - If the DNS client service is not enabled on the specified interface.