TCPIP_DNS_EVENT_HANDLER Type
C
typedef void (* TCPIP_DNS_EVENT_HANDLER)(TCPIP_NET_HANDLE hNet, TCPIP_DNS_EVENT_TYPE evType, const char* name, const void* param);
Description
Type: TCPIP_DNS_EVENT_HANDLER.
The format of a notification handler registered with the DNS module. Once an DNS event occurs the DNS service will be called for the registered handler.
Members
Members | Description |
---|---|
hNet | The interface on which the DNS event occurred. |
evType | The DNS reported event. |
name | The host name associated with the event. |
param | Additional user parameter - see TCPIP_DNS_HandlerRegister. |
Remarks
If pNetIf == 0, the notification is called for events on any interface.